Graphics Editor Properties Pane
Use the Properties pane to view and edit properties of the objects present in the work area.
Button | Description |
---|---|
![]() |
Normal
Click to display a selection of commonly used properties. |
![]() |
Detailed
Click to display all properties. |
Which properties are displayed in the Properties pane depends on the objects included in the graphic. Graphics properties define the appearance, boundary, and behavior of the graphic.